Technical FAQs

Ask a Question

Do the 9001 KU protective boots include a ring nut?

Yes. The standard ring nut is removed and the KU boot is installed with the 9001 K1 wrench.


CTA-ID : 2010208
Was this helpful?
What can we do to improve the information ?