Technical FAQs

Ask a Question

The cross reference program for a proximity sensor gives a multiple selection of sensors as possible replacements. Which should be used?

Occassionaly we offer several devices as replacements because there is a range of features on the original that are spread over several of the suggested replacements. It may be sensing distance, AC DC rating or possibly the material it is made of. The application must be considered to find the most suitable selection. Our cross reference tools are only a representation of the nearest matches that have a good probability of meeting the application needs. None of these should be considered an exact duplicate or unquestioned replacement.

CTA-ID : 2010204
Was this helpful?
What can we do to improve the information ?