Technical FAQs

Ask a Question

Does the ATV28 have an assignable Analog Output on the standard product?

Issue: Does the ATV28 have an assignable Analog Output on the standard product?  
 
Product Line:   ATV28
 
Environment:  All
 
Cause:   N/A
 
Resolution:   Yes, it does have Analog Output as a standard feature that can be programmed.

It can be programmed for;
     - no: not assigned
     - OCr: motor current. 20mA corresponds to twice the nominal motor thermal current ItH.
     - rFr: motor frequency. 20 mA corresponds to the maximum frequency tFr.
     - OLO: motor toque. 20 mA corresponds to twice the nominal motor torque.
     - OPr: power supplied by the drive controller. 20 mA corresponds to twice the nominal motor power.


 
Was this helpful?
What can we do to improve the information ?