Technical FAQs

Ask a Question

What is the IP rating on the remote mount keypad for the ATV28?

Issue:   What is the IP rating on the remote mount keypad for the ATV28?
 
Product Line:   ATV28
 
Environment:  All
 
Cause:  N/A 
 
Resolution:   It is rated IP65


 
Was this helpful?
What can we do to improve the information ?