Technical FAQs

Ask a Question

On the new Buck Boost slide rule calculators, the load column doesn`t read the same as the old calculators?<br />

The new (7414SP9901) now shows current (amps) instead of kVA, which allows for the maximum usage of the connection and the widest range of applied voltage. This matches the on-line buck boost calculator, which can be downloaded to a PDA or utilized on-line.


CTA-ID : 2010433
Was this helpful?
What can we do to improve the information ?