Technical FAQs

Ask a Question

What are the 3 phase connections for a 9036DG2?

A phase is wired to L1 T1
B phase is wired to T2 L2
C phase is connected direct to motor
Note: 9036DG2 wired as such is not a disconnect. For safety reasons a disconnect is required upstream in order to disconnect power to all 3 phases.


CTA-ID : 2010188
Was this helpful?
What can we do to improve the information ?