Technical FAQs

Ask a Question

What is the part number for the ATS46C32N SCR?

The SCR part number is  VZ3TM1400M16.

This is 1 SCR module. Two are required for each pole. There are six total in this size soft starter.




CTA-ID : 2009955
Was this helpful?
What can we do to improve the information ?