Technical FAQs

Ask a Question

SD Plug In Unit Enclosures

Issue:
Are enclosure only units available for the obsolete SD plug in units for obsolete SD Busway? 

Product Line:
Obsolete SD busway 

Environment:
Replacement

Cause:
Maintenance

Resolution:
Yes. The catalog numbers for the 4 pole enclosure-only devices (4 pole plug-in units mount onto 3 pole and 4 pole busway) are:
FAL circuit breakers use SD75400
KAL circuit breakers use SD78400  (Update: this is now obsolete with no replacement)
LAL circuit breakers use SD67400  (Update:  This is not system recognized, contact Technical Support for pricing and availability)



CTA-ID : 2025674
Was this helpful?
What can we do to improve the information ?