Technical FAQs

Ask a Question

What is the maximum signal frequency that can be used with the VW3A58202U option card for the encoder feedback?

The maximum signal frequency is 33 kHz with motor operating at drive controller high speed setting (HSP).


CTA-ID : 2010409
Was this helpful?
What can we do to improve the information ?