Technical FAQs

Ask a Question

What is the line voltage specification for the VSD07 and the overvoltage trip point?

The VSD07U... P10 = 120/208/240 Vac, 1-phase
             ``      ... P20 = 208/240 Vac, 1 or 3 phase
            ``       ... M20 = 208/240 Vac, 3 phase
            ``       ... N40 = 400/480 Vac, 3 phase
            ``       ... S60 = 590Vac 3 phase

The tolerance for this unit on all models is +10% / -15%




CTA-ID : 2010173
Was this helpful?
What can we do to improve the information ?