Technical FAQs

Ask a Question

Can you operate the ATV58 using BACnet protocol?

BACnet is not a protocol supported by SquareD or Schneider Electric for the Altivar 58 drive.
However, there gateway or bridge devices that can allow connection to a BACnet network by connecting to the drive using Modbus.

For Example: Automated Logic makes a device called PORTAL.
It bridges Modbus to BACnet.


CTA-ID : 2010170
Was this helpful?
What can we do to improve the information ?