Technical FAQs

Ask a Question

How do you order a QO330MQ150 with a QGL or QJL main circuit breaker provided, factory installed, instead of the standard QDL main circuit breaker?

Add a QGL or QJL suffix to the catalog number of the device, ie: QO330MQ150QGL or QO330MQ150QJL.


CTA-ID : 2009228
Was this helpful?
What can we do to improve the information ?