Technical FAQs

Ask a Question

How do you order a QO342MQ150 with a QGL or QJL main circuit breaker provided, factory installed, instead of the standard QDL main circuit breaker?

Add a QGL or QJL suffix to the catalog number of the device, ie: QO342MQ150QGL or QO342MQ150QJL.


CTA-ID : 2009229
Was this helpful?
What can we do to improve the information ?