Technical FAQs

Ask a Question

What is the CSA C22.2 No. 5-02 Canadian standard?

The CSA C22.2 No. 5-02 (equivalent to UL489) is the new CSA standard which replaces the No. 5.1. Both standards pertain to circuit breakers, not supplementary protectors. No. 235 (equivalent to UL1077) pertains to supplementary protectors.

CTA-ID : 2009225
Was this helpful?
What can we do to improve the information ?