Technical FAQs

Ask a Question

What are the dimensions of an A type hub?

The overall dimensions are 3.31`` x 3.31``. The mounting holes are 2.5`` center to center. The mounting holes are .25 diameter. Four 12-24 x 1/2`` mounting screws are provided.

CTA-ID : 2008982
Was this helpful?
What can we do to improve the information ?