Technical FAQs

Ask a Question

What is the part number for the Ethernet card for ATV58?

VW3A58310U
Version V2.1 and V1.1 Ethernet cards (VW3A58310U) are compatible with the following Altivar 58 (ATV58) drive controllers:
     ATV58, from V2.3 IE08
     ATV58 Type FVC, all versions
     The Keypad revsion must be higher than V3.0


CTA-ID : 2005471
Was this helpful?
What can we do to improve the information ?