Technical FAQs

Ask a Question

Can the VW3A66201T still be obtained because system refers you to alternate VW3A66201AT for the 24v I/O extension card for that ATV66?

If there is stock available and a third analog output is required, you can purchase the VW3A66201T which includes an AO3 for use.
The system message suggests an alternate VW3A66201AT in case of a stock outage or Analog Output 3 is not required.


CTA-ID : 2005399
Was this helpful?
What can we do to improve the information ?