Technical FAQs

Ask a Question

Customer asks if the base channels are required for mounting a QED2 switchboard on a housekeeping pad?

Per Larry of the Columbia TAG, customer was advised that the switchboard can still be bolted down without the base channels but there are no instructions because it is not the normal way.


CTA-ID : 2009223
Was this helpful?
What can we do to improve the information ?