Technical FAQs

Ask a Question

Is there a separate NEMA 1 general purpose enclosure for field assembly for the Class 2510 Type F & K controllers?

Yes, There are (3) options:
(1) Class 9991 Type EN1 - Standard
(2) Class 9991 Type KE1 - Oversized
(3) Class 9991 Type KE2 - Jumbo


CTA-ID : 710
Was this helpful?
What can we do to improve the information ?