Technical FAQs

Ask a Question

What are the dimensions of an A-L type hub?

The overall dimensions are 5.0`` x 5.0``. The mounting holes are 4.0`` center to center. The mounting holes are .312 diameter. Four 1/4-20 x 1/2`` mounting screws are provided.


CTA-ID : 2008940
Was this helpful?
What can we do to improve the information ?