Technical FAQs

Ask a Question

What is the part number for the ring nut for a 9001SKRU11?<br />

9001SK41. This is also the ring nut used in a 9001 SKR1 , SKR12 (momentary button only), SKR4 , SKR5 , and SKR9 .


CTA-ID : 2008978
Was this helpful?
What can we do to improve the information ?