Technical FAQs

Ask a Question

What is the maximum mains rating amperage available in a HOMELINE load center?

Issue:
Product Design Features

Product Line:
Homeline Load Centers

Environment:
Maximum Mains rating

Cause:
Application

Resolution:
The maximum mains rating amperage for the Homeline load centers 225 ampere Maximum. For higher amperages, consider a QO load center or NQ panelboard.


CTA-ID : 2008977
Was this helpful?
What can we do to improve the information ?