Technical FAQs

Ask a Question

Can you use a QO240GFI on a single phase load?

Yes. Wire the load hot wire to the right pole, and the load neutral to the labeled terminal on the breaker. The ground fault push to test button uses the right hand pole.


CTA-ID : 2008970
Was this helpful?
What can we do to improve the information ?