Technical FAQs

Ask a Question

What is the part number for the status monitor and the monitor board for the Omegapak 8804 because MC-21 does not come up in the system?

These components and the 8804 drive they are part of is obsolete, but the part number is 8804 MC-21 which is the only part number available for the status monitor kit. The kit includes the monitor and the board.

Need to go through a distributor whom can contact Dave Hamline at the obsolete product Depot Repair Facility in Crown Point, IN to inquire about part availability, repair or replacement on the unit in question.

CTA-ID : 4110
Was this helpful?
What can we do to improve the information ?