Technical FAQs

Ask a Question

What circuit breaker enclosure will accept a KIL circuit breaker?

The KIL circuit breaker can be mounted in the IK250DS (NEMA 1, 3, 3R, 4, 4X, 5 or 12 applications), or IK250AWK (NEMA 1, 3R, 5 or 12 applications).


CTA-ID : 2009472
Was this helpful?
What can we do to improve the information ?