Technical FAQs

Ask a Question

What circuit breaker enclosure will accept a KAL circuit breaker?

Issue:
Product availability

Product line:
Circuit breaker enclosures

Cause:
application

Resolution:
ALL THE KA ENCLOSURES ARE OBSOLETE, NO LONGER AVAILBLE, WITH NO DIRECT REPLACEMENT. NEED TO CONSIDER THE PowerPact J Frame breakers with J Enclosures.

The KAL circuit breakers(225Amp Maximum) were used in the following enclosures:
1) KA225F (NEMA 1, flush mount applications).
2) KA225S (NEMA 1, surface mount applications).
3) KA225RB (NEMA 3R applications).
4) KA225DS (NEMA 1, 3, 3R, 4, 4X, 5 or 12 applications).
5) KA225A (NEMA 12K application).
6) KA225AWK (NEMA 1, 3R, 5 or 12 applications).
7) KA225X (NEMA 7 applications).
8) KA225Y (NEMA 9 applications).

 
Was this helpful?
What can we do to improve the information ?