Technical FAQs

Ask a Question

What are the dimensions of an 8911DPSO63, DPSO73, and DPSO93?

The 60-90A range definite purpose starters are 5.32``W x 11.05``H x 5.68``D (from reset button to back).


CTA-ID : 2008955
Was this helpful?
What can we do to improve the information ?