Technical FAQs

Ask a Question

What is the terminal lug data for the GJL36015 thruough GJL36100?

One #14 AWG to #1/0 AWG Cu, or one #8 AWG to #1/0 AWG Al.


CTA-ID : 2008952
Was this helpful?
What can we do to improve the information ?