Technical FAQs

Ask a Question

What is catalog number of the TeSys overload relay that can be used on single phase loads?

The complete catalog number will depend on the motor nameplate full load current, but the prefix of the overload is LR3D. These are now available for both Class 10 and 20.

CTA-ID : 2008949
Was this helpful?
What can we do to improve the information ?