Technical FAQs

Ask a Question

Do we have a different neon lamp for the XB4 or XB5 units? The standard bulb is dim.

Neon lamps are dim especially if used at a lower voltage than nominal. Neon is old technology that was used because they lasted longer than incandesents. For better illumination suggest incandesent or for long life LED.

CTA-ID : 2008771
Was this helpful?
What can we do to improve the information ?