Technical FAQs

Ask a Question

Is the 2510 Type K manual switch UL Listed?

The 2510 KR has the same approvals as the 2510 type F manual starter which is UL Listed under File #E42243 CCN NLRV for enclosed and for explosion proof file number is E58760 CCN NPXZ. The open style devices are UL Recognized.

CTA-ID : 2004838
Was this helpful?
What can we do to improve the information ?