Technical FAQs

Ask a Question

What circuit breaker enclosure will accept a FCL circuit breaker?

The FCL circuit breaker can be mounted in the FA100F (NEMA 1, flush mount applications), FA100S (NEMA 1, surface mount applications, FA100RB (NEMA 3R applications), FA100DS (NEMA 1, 3, 3R, 4, 4X, 5 or 12 applications), FA100A (NEMA 12K application) or FA100AWK (NEMA 1, 3R, 5 or 12 applications).
NOTE: The FCL circuit breaker can also be mounted in the next larger size enclosure KA225F (NEMA 1, flush mount applications), KA225S (NEMA 1, surface mount applications) or KA225RB (NEMA 3R applications).

CTA-ID : 2009466
Was this helpful?
What can we do to improve the information ?