Technical FAQs

Ask a Question

What circuit breaker enclosure will accept a LAL, LHL or Q4L circuit breaker?

Issue:
Selection

Product Line:
Circuit Breaker Enclosure

Cause:
Selection

Resolution:
The LAL, LHL or Q4L circuit breakers can be mounted in the LA400F (NEMA 1, flush mount applications), LA400S (NEMA 1, surface mount applications, LA400R (NEMA 3R applications), LA400DS (NEMA 1, 3, 3R, 4, 4X, 5 or 12 applications) or LA400AWK (NEMA 1, 3R, 5 or 12 applications).


CTA-ID : 2009457
Was this helpful?
What can we do to improve the information ?