Technical FAQs

Ask a Question

What is the ``J`` in the KCJ34225?

It is a special strap connector built for IEM Switchboards/Switchgear. This special strap connector is also available on the FA, FH, FC, FI, KA, KH, KC, KI, LA, LH, MA, MH, NA, and NC breakers.


CTA-ID : 2008946
Was this helpful?
What can we do to improve the information ?