Technical FAQs

Ask a Question

Can you series rate a NQOD panel with the QB,QD,QG,and QJ breakers?

Yes, Series ratings are available with the QD,QG, and the QJ breakers. Refer to Digest pages 8-2 and 8-3 or the information manual provided with the panelboard.


Revised 3/10/04



CTA-ID : 2008942
Was this helpful?
What can we do to improve the information ?