Technical FAQs

Ask a Question

What lugs are available for use on a UTH7300T?

Lug Kits available include:
ARP00118 - includes one, two barrel lug for #6 AWG - 250 kcmil (al/cu)
ARP00129 - includes one, single barrel lug for #4 AWG - 600 kcmil (al/cu)
ARP00427 - includes three, two barrel lugs for #6 AWG - 250 kcmil (al/cu)


CTA-ID : 2008750
Was this helpful?
What can we do to improve the information ?