Technical FAQs

Ask a Question

What is the Terminal Lug Data for a H227N, H227NR or H227NAWK Heavy Duty safety switch?

The lugs on this device will accept (3) #3/0 AWG - 750 kcmil aluminum or copper conductors per phase and neutral.


CTA-ID : 2009442
Was this helpful?
What can we do to improve the information ?