Technical FAQs

Ask a Question

What is the Terminal Lug Data for a H327N, H327NR or H327NAWK Heavy Duty safety switch?

Product Feature

Product Line:
Safety Switch

Clarifying lug wire range

The lugs on this device will accept (3) #3/0 AWG - 750 kcmil aluminum or copper conductors per phase and neutral.

CTA-ID : 2009444
Was this helpful?
What can we do to improve the information ?