Technical FAQs

Ask a Question

What parts are included in the Magelis terminal for the ATV28 and ATV58 part number XBTHM017010A8? <br /><br />What other componets are required for connection?

The Magelis terminal has the HMI application pre-loaded and the XBT-Z908 cable to go to the TSXSCA62 Hub from the display.

When connecting to the ATV28 order the following:
TSXSCA62 (hub) includes 2 - db15 (female) connectors
VW3A58306U (cable) db 15 (male) to db 9 (male)
VW3A28301U (cable) db 9 (female) to RJ45
For proper selection of the qty of TSXSCA62 needed for your installation please contact PSG or Sales

When Connecting to the ATV58 order the following:
TSXSCA62 (hub) includes 2 - db15 (female) connectors
VW3A58306U (cable) db 15 (male) to db 9 (male)
For proper selection of the qty of TSXSCA62 needed for your installation please contact PSG or Sales


CTA-ID : 2009439
Was this helpful?
What can we do to improve the information ?