Technical FAQs

Ask a Question

Does Sq D offer a turnstile limit switch with snap action contacts ?

Use a XCRE18 for a DPDT switch with both contacts operating when the lever rotates 65 degrees from center. The switch can rotate 90 degrees left or right of center, but cannot continue through a full 360 degree.

CTA-ID : 2009143
Was this helpful?
What can we do to improve the information ?