Technical FAQs

Ask a Question

Do the 8501CO type relays have continuous duty rated coils?

Issue:
Do the 8501CO type relays have continuous duty rated coils?
Product Line:
General Purpose Relays 
Environment:
Square D Power Relays
Cause:
Application is calling for continuous duty rated relay.
Resolution:
Yes, they are continuous duty rated.
Was this helpful?
What can we do to improve the information ?