Technical FAQs

Ask a Question

Can the QO13040L200GRB load center be converted to a main breaker device?

Yes, the load center can be converted by field installing a Main Breaker Kit, from 100 ampere minimum through 200 ampere maximum. Use QOM2200VH for a 200 ampere main breaker application.

CTA-ID : 2009179
Was this helpful?
What can we do to improve the information ?