Technical FAQs

Ask a Question

What is the input line voltage specifications for the ATV28 unit?

ATV28****M2U, 1-phase 208 V -15% to 230 V +10%
ATV28****M2U, 3-phase 208 V -15% to 230 V +10%
ATV28****N4U, 400 V -15% to 460 V +10%

This information is available in the Electrical Characteristics table in the User`s Manual.


CTA-ID : 2009167
Was this helpful?
What can we do to improve the information ?