Technical FAQs

Ask a Question

What`s the difference between an FAL breaker and an FAP breaker?

The FAL breaker has lugs on the Line (ON end) and Load (OFF end) side and the FAP breaker has lugs on the Load side (OFF end) only.


CTA-ID : 2009166
Was this helpful?
What can we do to improve the information ?