Technical FAQs

Ask a Question

What replaces the Q1290 breaker used in obsolete Vertical EZ Stack multi-metering device?

Issue:
Old product repair parts

Product Line:
EZ Stack Metering

Environment:
Tenant Breaker

Cause:
Maintenance

Resolution:
The 100 ampere Vertical EZ Stack devices accepted either QO (through 70 ampere) or Q1 (70 - 100 ampere) tenant breakers. ALL the Q1 type of breakers are Obsolete and no longer available. The Q1290 can be replaced with a QO290.


CTA-ID : 2009163
Was this helpful?
What can we do to improve the information ?