Technical FAQs

Ask a Question

Can the PLC communication module be used in addition to the keypad?

No. The PLC communication module (VW3G46301U) is to be installed on the main control board where the keypad display is normally installed. It is not possible to use a keypad when the communication option is installed. Information normally entered and retrieved by the keypad display can be accessed by means of the serial communications.

CTA-ID : 7342
Was this helpful?
What can we do to improve the information ?