Technical FAQs

Ask a Question

Where is the Short Circuit Rating of a Homeline load center located?

The Short Circuit Rating information is located on the box label, which is normally affixed on an inside wall of the load center.


CTA-ID : 2008711
Was this helpful?
What can we do to improve the information ?