Technical FAQs

Ask a Question

Can a Homeline load center be series rated with upstream fuses as the remote main?

Issue:
Product Features

Product Line:
Homeline load centers

Environment:
Short Circuit Current Ratings

Cause:
Application

Resolution:
No, This would be considered a 2-Tier Series Rating and the Homeline load centers do NOT Series rate with a remote main Fuse.


CTA-ID : 2008704
Was this helpful?
What can we do to improve the information ?