Technical FAQs

Ask a Question

How do the closing plates mount on the adapter going from the old LD wireway to the new LDB?

The new closing plates will fit the old duct, however the holes do not line up. The customer will need to drill new holes in the LDB wireway.


CTA-ID : 15015
Was this helpful?
What can we do to improve the information ?