Technical FAQs

Ask a Question

Does the PEF breaker faceplate tell the amperage of the breaker?

There is a label that states the sensor size. There is a label that states the configuation as shipped from the factory: amperage and installed rating plug. There is also a label that states the amperage the breaker will be with other rating plugs installed. This is true for all MICROLOGIC Series B trip units. The Long Time dial setting, rating plug, and sensor size all contribute to the amp rating.


CTA-ID : 2009138
Was this helpful?
What can we do to improve the information ?